Other Parts Discussed in Thread: UC1843B-SP
I'm looking to use TPS50601A-SP as a POL converter to generate 1.2V, 2A output power from 5V input voltage. Based on the various references designs and eval board documentation I've come across, it seems like the smallest solution size using this device is about 0.8 to 1 in^2.
I'm wondering if it's possible to get the solution size under 0.5 in^2 or if there are any other recommendations for a rad-hard power solution that can provide the smallest solution size.