Other Parts Discussed in Thread: LMR14050
What is the effect if no soft start capacitor is installed which the datasheet says limits inrush current. My power supply is fed by mains, the 18VAC secondary is rectified and feeds 5400uF, so it seems power-on inrush current to the LMR14050 would be minimal or zero because the bulk filter capacitors would absorb it all. But, if the LMR14050 is disabled during operation there could be some inrush current depending on the load when the LMR14050 becomes again enabled. Would this cause a deleterious effect in the LMR14050?