Tool/software: WEBENCH® Design Tools
Calibrate output voltage and use the method as follow: VOUT_CAL_GAIN = 100*[(Vout1-Vout2)/(Read_vout1-Read_vout2)-1]. VOUT_CAL_OFFSET = Vout3 - Read_Vout3. For meet the requirement, set the load to 6A and the full load is 12A. But I found that the gain whcih I calculate is not in the limit. The limit in the datasheet is -0.125---+0.121%. Why?