This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: BQ34Z100

Part Number: BQ34Z100
Other Parts Discussed in Thread: EV2400

1. I test the voltage,when VCC is 3.3V,then REGIN is 2.1V,but BQ34Z100 need 2.7~4.5V for REGIN, BQ34Z100 does't work. Could I delete R75,D13 and Q15 ?

2. The same I2C line is pulled up to 3.3V, will it impact BQ34Z100 communicate through EV2400 to computer?