Hi everyone,
I've designed a PCB and now I am in the process of testing. I have combined the battery protection IC BQ29707 with the battery fuel gauge BQ27421 and a wireless charging IC BQ51050.
My problem is that when I connect the Li-Ion battery I get strange behavior... I measure around 1V at the output (actually it is fluctuating 1.0 - 1.1 volts)... As soon as I turn on the wireless charging then I am able to measure the correct voltage around 4.2 - 4.1 volts. Even after I disconnect the wireless charging, I keep measuring the correct voltage. When I disconnect the battery and connected back I have the same problem..
It is very strange, it is like the MOSFETs (U11 & U12) turns on as soon as I connect the wireless charging...
These are the schematics for battery protection, battery fuel gauge, and wireless charging. I believe that the problem somehow lies in battery protection but I cannot figure out what is going on. Also, I place a diode (D2) for reverse polarity protection which I have removed now to avoid the voltage drop. It is like the Mosfets turn on only when I connect the wireless charging but I do not know how this is related.
Any suggestion?