This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76701-EP: Confirmation of Operating/Abs Max Tj and Tshutdown

Part Number: TPS76701-EP


Hello, 

The datasheet says that the recommended operating/abs max temp is 125C. However, the thermal shutdown temperature is rated at 150C. 

Can we please ask for confirmation if 150C is the correct value? 
If it is, then the device will not shut down even if exceeds the absolute maximum of 125C?

Thank you very much.

Regards,
Elisha