The data sheet of the L5045 provides for the connection of Vdd to Vcc to facilitate the use of an external regulator for high voltage. According to the data sheet a voltage greater than 10v should enable the operation of the IC when Vdd is connected to Vcc. Otherwise, the data sheet indicates that at least 14 volts need to be applied to Vdd when Vcc is not connected to Vdd. The PSpice model does not allow soft start to being charging with 10.5v applied to Vdd and Vdd when Vdd and Vcc are connected together, nor does it produce outputs including the function of the ramp connection.
I would like to use this part for a requirement that provides a 12V-36V power source. According to the behavior of the PSPICE model this is not possible as, according to the PSPICE mode, at least 14V needs tp ne applied to Vdd for the IC to work while my application would require that it work with as little as 12V. My design at present provides for a low dropout voltage regulator which provides 10.5 volts to the circuit that connects Vdd to Vss.
Please let me know if my design should work. Does the LM5045 part able to operate properly with as little as 10.5 volts applied to Vdd and Vcc when Vcc and Vdd are connected together even though it's Spice model does not operate under these conditions.
Also, I believe it should be very easy fix the model. Please let me know when the model is repaired.
Thank you very much,
David Fiori, Jr.
215-584-2214 (cell)