Part Number: BQ20Z95
Hi there,
I am working on a sealed pack based on bq20z95 for cycling. I could temporarily unseal and with fully access by 0414 3672 and ffff ffff. Then I could update the configuration and import/export GG file and re-program with default bq20z95 dfi file. However, this chip will get back to sealed condition after Reset the chip. I don't know when I finally export the ROM file, the sealed condition (or mark) will or will not bring into the ROM file?
So if the chip could be Permanently unsealed, it would great.
Another issue I need your help: I could not find the Chem ID in the Chemistry List in bqEV software. The battery part number is LGABF1L1865 3350mAh
Thanks,
Paul