This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: Current sense is inverted, discharging sets the BatteryStatus.CHG bit.

Part Number: BQ34110EVM-796
Other Parts Discussed in Thread: BQ34110, BQSTUDIO

The current sensing polarity is inverted. Charging is Negative current and Discharging is positive current. I have battery and load (resistor) connected as in Figure 1 of the bq34110EVM Quick Start Guide.

I replaced the bq34111 IC. During charging the BQ34110 [DSG] flag is set and the gauge indicates a negative current in bqStudio 1.3.86. Similarly to charging, discharging incorrectly causes the [CHG] flag to set. When I apply a 350mA load for calibration, specifying -350 mA applied current results in the gauge adjusting to +350 mA.

I do believe I initially set current Positive during calibration, but now when I do calibration with a negative current (and discharging), it will not return to normal. I have tried re-flashing firmware (bq34110_v0_02_build_9.srec) twice; no change.