Other Parts Discussed in Thread: TINA-TI
Dear Tuan, please answer
I need 1 A output current.
I have 10 - 30 V input voltage. I plan to set the output voltage to 36 - 40 V.
QUESTIONS:
1) How do you think, I can use TPS92692 or I can take another chip with fewer external elements? Please, advise, that there is still.
2) If I set 36 V output, then it is "boost driver" ? (Input voltage 10 - 30 V.)
3) Is it possible to set 12 V output voltage? (Input voltage 10 - 30 V.)
4) Plase, remind how to convert PSpice model to TSC ? I'd like to simulate boost driver in TINA-TI. Please see attach.
TIA.
Sincerely,
Vladimir Naumenkov