Hello there
I see that the withstand voltage of the HO port of the LM5035 is 105V.
If the power supply Vin is 100V and the PWM drive voltage is 10V, then the maximum voltage of the HO port will reach 110V, will it damage the HO port?
So how can the LM5035 be used to ensure that the PWM drive voltage reaches 10V when Vin is 100V?