Hi,
Can LM3017 be used as a high side switch with True Shutdown? In our application, we really need to minimise shutdown current and keep it in the nanoamp range.
My thoughts are as follows.
- Remove L1 and D1 (from the typical application circuit).
- Keep Enable ≤ 0.4V for shutdown mode.
- Keep Enable ≥ 2.6 V for passthrough mode.
But
- What should we do with the Feedback pin?
- How can we disable current limiting so that this high side switch can work with a high current power FET (N-channel) ? Or can we trick it into never seeing overcurrent?
- Will any of the above have a negative effect on shutdown and operating/quiescent current?
The 40nA shutdown current is far too good to pass up. However, the 1µA maximum is enough to rule it out.
Can you please tell me what factors could cause LM3017 to go from 40nA to 1µA in shutdown so that we can evaluate where it would mostly sit?
Please know that I'm still going to continue my other thread about high side switches because something better may still come from it. If I'm wrong about how LM3017 works then I don't want to derail that thread since I still need help. https://e2e.ti.com/support/power-management/f/196/t/895959