This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: discharge issue at -20 degree

Part Number: BQ27542-G1


Hi Team,

we use GPC to get the report,but the pack directly discharge RSOC at -20 degrees,and the RSOC is about 8x% and directly to 0%, 

and the customer system can not turn on at -20 degree,so what happen to cause this problem? there problem with the battery specificaion?

please kindly refer the attached.

ICP535172AWRU pre spec_STD(4.4V)160928.pdf

AKH08-20200422.gg.csv

AKH08-(-20C)放置LOG.xlsx

AKH08_GPC_Rb.zip

AKH08_GPC_Chem ID.zip

AKH08_GPC_Chem ID-report.zip

AKH08_GPC_Rb-report.zip