Hi
My device has 1 cell Li-Po battery, and the required power is 5V, 3.3V, 2.8v, and 1.8V.
1. if the boost operation of BQ25616 is enabled, which pin of BQ25616 is used to supply the boosted 5V,1.2A power ?
2. Can I use this boosted power for my device, or other device ?
3. When the power is supplied from battery in the boost mode, the VSYS voltage is also 5V ?
if not 5V, is the voltage on the VSYS pin the the one of battery ?