Hi team,
My customer is using TPS3828-33 to monitor MCU. They met below issue,
when customer let MCU work in low power mode, WDI cannot go to high ipedance state. This will trigger the reset pin to low output. Whta they do now is to pull WDI pin with 50k resistor to 3.3V, this can solve their probelm.I want to check with team that if this is ok to use?
I also see the same issue in below thread, I am thing to let the WDI pin of the MCU into input IO to let TPS3828 into Auto-Reset Oscillator state. Can this method solve this issue? Thank you for your help here.
BR,
CL
https://e2e.ti.com/support/power-management/f/196/p/734710/2713411?tisearch=e2e-sitesearch