This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to connect this load switch to a RC load with the capacitance value of 10pF. Is it possible to use to this load switch (I need to understand the off capacitance offered by this device) because whenever the switch is off (O.C.) the RC will be charged by a 3.3V rail. I do not want the rise time to be impacted by the load switch.
Thanks,
Aishwarya
Hi Aishwarya,
Welcome to E2E!
I have a questions to help me further understand the application to see if the TPS22910A can be used. If the RC load can be powered by a different 3.3V rail what is the load switch going to be used for? Could you further elaborate on the application and functionality of this part of the system?
Best regards,
Andy Robles