supply voltage : 3.3V
When VLOAD<60V, ILAOD<100mA;
When VLOAD≥60V, ILAOD ≈ 400mA;
The use of dry battery power, not connected to the load when the current is so large, can not be used normally, there is a way to make the current down to the normal range? tks!