This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155: ILOAD overcurrent issue

Part Number: LM5155

supply voltage : 3.3V

When VLOAD<60V, ILAOD<100mA;

When VLOAD≥60V, ILAOD ≈ 400mA;

The use of dry battery power, not connected to the load when the current is so large, can not be used normally, there is a way to make the current down to the normal range? tks!