Hi Team,
I have questions and a request.
- Can you provide the Fsw formula by using RT formula on the datasheet section 7.3.5?
- When customer use 400kHz frequency, what combination is the best for their design in the minimum variation stand point?
- According to the figure 1 of the datasheet, we can see several Rt-C combination. In general, lower capacitance and resistance is less variation than bigger value. However, the relation between Rt and C is like inverse proportion. Therefore we want to understand what the combination should be the best.
- Does this device have pulse skip mode? If no, could you tell me the operation, when the on time is less than minimum pulse width?
Thanks,
Uchihara