Other Parts Discussed in Thread: UCC29002, , UCC39002
hi
where the + sense input marked in the picture should be connected in the ucc28950 IC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm not sure that I understand your question but
The UCC39002 increases the output current of the module it is attached to by sinking a current at its ADJ pin through the NPN transistor. This current causes a voltage drop across RADJUST which 'fools' the UCC28950 controller into thinking the output voltage is lower than it should be. The UCC28950 then increases the module output voltage (by a small amount of course) to increase the output current. All of the UCC39002 controllers are using the same voltage at the LS bus as their reference so the currents are forced to be equal.
If that's not the answer you need then please let me know.
Regards
Colin
Hello
Yes it will - assume you need to provide about 500mV of Vout trimming. Iadj can sink up to 4mA (approx) so RADJ = 500mV/4mA = 125 Ohms. - remember there is almost no current flowing in the output voltage sensing network of the controller. This is a VERY QUICK calculation but the principal is clear. There is an Excel calculator tool available on the product web page at https://www.ti.com/lit/zip/sluc684 that will guide you through the design process.
Regards
Colin
Hi
It looks like our messages crossed - 6mA is the DS value - the 4mA value I used in the example was wrong (I should have checked the DS first !)
Here's a link to a presentation on the UCC29002 /cfs-file/__key/communityserver-discussions-components-files/196/8358.Load-Share_5F00_V1.pptx
Regards
Colin
Hi
I'm not sure that I understand your question but
The UCC39002 increases the output current of the module it is attached to by sinking a current at its ADJ pin through the NPN transistor. This current causes a voltage drop across RADJUST which 'fools' the UCC28950 controller into thinking the output voltage is lower than it should be. The UCC28950 then increases the module output voltage (by a small amount of course) to increase the output current. All of the UCC39002 controllers are using the same voltage at the LS bus as their reference so the currents are forced to be equal.
If that's not the answer you need then please let me know.
Regards
Colin
can you elaborate a little more i think i don't understand
Hi
Let's say the ADJ pin sinks 2mA. This current flows in RADJUST and causes a voltage drop of RADJUST*IADJ - so let's say 150 Ohms * 2mA = 300mV. The UCC28950 controller will control the voltage at the left hand side of the RADJUST resistor (Vsense in my diagram above ) to be 28V but in order to get 28V at Vsense the output must be regulated up (by the UCC28950 controller) to 28.3V.
The UCC29002 controller can force equal current sharing by slightly adjusting the output voltages of the PSUs in the system so that they are each forcing equal current.
I'd suggest you take some time to look over the .pptx file I posted earlier to try to see if all this makes sense or not (hopefully it should make sense) slide 17 and 18 show RADJ with the voltage drop across it due to IADJ.
Regards
Colin
Hi
I'm glad I was able to help - I'm closing this thread now. Feel free to open a new - linked - thread if you have any further questions.
Regards
Colin