Dear all,
I would like to ask about short circuit protection of TPS621361.
When I checked 9.4.5 Current Limit And Short Circuit Protection in the data sheet, the following notation was found.
I have two questions about the above.
① Does the above notation mean, "When overcurrent is detected, the current limit is applied, but the internal high side switch does not turn off"?
②Please answer if ① is YES.
I have a perception that when the TPS621361 detects an overcurrent, it does not become 0V (the output does not stop) over time. Is this correct?
Best Regards,
Y.Ottey