Part Number: LM5116
Hi sir/Madam.
we have requirement for single phase (Single LM5116) Buck converter with 380W output power.
Previously we have worked with PMP2782 and we have observed the 27A load sharing in one phase of 2-phase Interleaved converter for 50A load for same LM5116 IC and now, we are planning to use LM5116 for 380W requirement.
Our requirement is as follows:
Vin: 15V to 42V
Efficiency: > 90%
Load current: 30A
So, please support us for the following queries regarding LM5116.
- what is maximum power capability?
- Currently, we are using IC for 300W. if we use this IC for more than 300W, what are the major components that have to be changed?
Regards,
Khagesh