This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir/Madam.
we have requirement for single phase (Single LM5116) Buck converter with 380W output power.
Previously we have worked with PMP2782 and we have observed the 27A load sharing in one phase of 2-phase Interleaved converter for 50A load for same LM5116 IC and now, we are planning to use LM5116 for 380W requirement.
Our requirement is as follows:
Vin: 15V to 42V
Efficiency: > 90%
Load current: 30A
So, please support us for the following queries regarding LM5116.
Regards,
Khagesh
Hi,
LM5116 is a buck controller and the maximum power capability is determined by the power MOSFETs you choose. If you want to have a higher output power, at first you need to check if the MOSEFTs can endure the current, if not you need to change high-current rating MOSFETs, at the same time you need to check the drive current requirements of new MOSFETS and driver capability of LM5116. Thanks.