Other Parts Discussed in Thread: TPS54340, TPS54341
Tool/software: WEBENCH® Design Tools
Dear Sirs,
We used TPS54240 DC/DC converter in our old design. It has a good cost and is widely used us. Our design contains two power supplies: 12 – 36V primary power source and 7V reserved secondary power source. I want to set TPS54240 DC/DC converter to Vout = 12V, the maximum load current is 2A. Us I understand from TPS54240 datasheet to improve drop out, the TPS54240 is designed to operate at 100% duty cycle as long as the BOOT to PH pin voltage is greater than 2.1 V. As I understand as duty cycle is 100% then minimum input supply voltage Vin min is near the output voltage Vout of the application.
I have some questions about TPS54240 operate:
1) I tried to simulate TPS54240 at Vin = 12 – 36V, Vout = 12V, Iout max = 2A mode in webench designer. Webench designer allows to set Vin min = 13,2V only. What will the really output voltage Vout, if Vin really = 12V and TPS54240 will be configured at Vin = 13,2-36V, Iout=2A, Vout = 12V? Can I legally use TPS54240 in this mode for a long time, if Vin really = 12V and TPS54240 will be configured at Vin = 13,2-36V, Iout=2A, Vout = 12V?
2) If 12 – 36V primary power source is absent, then reserved secondary power source is 7V. What will the really output voltage Vout, if Vin really = 7V and TPS54240 will be configured at Vin = 13,2-36V, Iout=2A, Vout = 12V? Can I legally use TPS54240 in this mode for a long time, if Vin really = 7V and TPS54240 will be configured at Vin = 13,2-36V, Iout=2A, Vout = 12V? I understand, that TPS54240 is buck converter and Vin really = 7V less then Vout = 12V. But Vin really = 7V and Vout really = 7V is normal for my task, although TPS54240 will be configured at Vin = 13,2-36V, Iout=2A, Vout = 12V.
3) Must I use buck-boost converter for my task necessarily?
4) Can I use other TI buck converters for my task? What TI buck converter can I use for my task (part number)?
Best regards,
Ruslan.