Hi Sir,
We are now testing TPS2546 for usb charging.
the laptop set TPS2546 as 1111 CDP mode, the RILIM_Hi is 20KΩ;
when plug usb device(VIVO cellphone) to start charging, the charging current is only 0.886A; even when we adjust RILIM_Hi from 20K to 9.1K, the current is as the same as 0.886A.
Then set RILIM_Hi to 81.9K; output charging current is down to 0.477A.
check (Vin-Vout)/Iout=(4.98-4.9)/0.886=90mΩ, Close to the typical value(73mΩ);
according to Equation 1 in datasheet, the out put current value is abnormal.
Please help to check it, thanks very much.