This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Qianqian,
If the device will be operating at or close to room temperature, and you choose the correct package, then yes this will work.
The watts dissipated across the device is (24-3.3)*(200mA) = 20.7*0.2 = 4.14 watts.
The thermal resistance (junction to ambient) for the KC and KCS package is 19 C/W.
So the temperature rise is 4.14 W * 19 C/W = 78.66C.
If room temperature is 25C then the total temperature is 25 + 78.66 = 103.66C.
The device is rated to operate at 125C, so you have around 20C of margin.
Thanks,
- Stephen