This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33610: HS FET,LS FET Resistance

Part Number: LMR33610
Other Parts Discussed in Thread: LMR36510, LMR33620

Hi TI,

I want use new design LMR33610ADDAR,

Design Requirement is

Input voltage is 30V and Current is 150mA,

and output volatge of buck regulator is 5V and current is 300mA.

for this i am planing to use LMR33610ADDAR Buck regulator ,

I want to calculate the Power losses like switching losses and conduction and inductor losses so i need the RDS values of HS side and LS side of Fet ,

In datasheet that details not provided please provide the Rds  value and Please provide the Suitable inductor part number.