This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
I'd like to confirm the differences between TPS54202 vs TPS54202H.
From my understanding,
1: The device has SSC or not.
2: The device has an internal pull-down 1Mohm or not.
and EN hysteresis current looks different, is this because of the 1Mohm resistor?
Best Regards,
Kazuki Kitajima
Hi Kazuki,
Yes, your understanding is correct. TPS54202H disables SSC function for some applications that require fixed frequency(like surveillance) and there are changes on the EN related circuits to realize the feather that float EN pin to disable IC, so that hysteresis current looks different.
Thanks.
BRs,
Bruce
Bruce-san,
Understood.
Thank you for your answer.
Best Regards,
Kazuki Kitajima