This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5035C: doubt about LM5035 version change

Part Number: LM5035C
Other Parts Discussed in Thread: LM5035,

Hello,
I see the LM5035C manual has a comparison of the functional differences between the LM5035 versions, as shown below:

Among them, the latest LM5035C and the original LM5035 are opposite in terms of "SR state in UVLO shutdown and Hiccup current limit" and "soft-stop after UVLO".

I do n’t know why such a change was made?

When I was using the LM5035 recently, when I encountered light load or no-load shutdown, the secondary SR drive has been turned on, resulting in a reverse output current and a 100V voltage spike on the SR. Is it possible to use the LM5035C? When light load or no load, turn off the drive signal of SR in time, so as to avoid the output current reverse flow and the generation of spikes on SR?

Thank you.