Other Parts Discussed in Thread: UCC28951
Hi!
Some time ago I've been asking some questions about UCC28950.
Now I get real converter hardware for first run and testing.
Basic parameters are:
Full power 5kW.
Input 18-36V.
Output 400V (making test on 100V only for safety by changing feedback gain).
Frequency 50kHz.
Bridge is made with 16 MOSFETs by 4 MOSFETs in parallel.
There are 3300uF and 700uH output filter.
I have some doubt about correct working of current sensor. It's LEM505 with inverting OpAmp for scaling and rectifing as in TI Analog Engineer's cookbook, p. 70 ;)
I tried to start the converter without current feedback, but with only 50W load it gets unstable work with noise, big current transients and huge voltage spikes on MOSFETs.
Is it possible to run UCC28950 with voltage feedback only?
Now I want to test power capabilites and make some other tests. I don't need fast reaction on transients and full functionality.
P.S. I tried to run converter without any feedback - it's works correctlyff with 100% duty.