I have a problem with the TPS2378DDA device
Vin- 48V
Current ~400mA
· When they connect the system to DC in line it is working O.K. (POE is disconnected).
· When they connect the system to POE (DC in is disconnected) with load the power is fluctuating.
Please help me to understand where is the problem.
Thanks,
Oved