This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kazuto, recommend to use 0.68uH as default.
Yuchang
Hi Kazuto,
You can check the curve of inductor value & current, for SPM6530T-R68M140, when current is close to 16A, inductor value will drop to around 0.5uH, and for R47-0.47uH, it is about 0.39uH@16A, so SPM6530T-R68M140 looks better.
Yuchang
Kazuto,
IC sense valley of current ripple to trigger OCP, in my opinion, the peak value should not impact the OCP, even it has, it should be a little. and also you can see the inductor VS current curve is for DC current not peak current.
Yuchang