This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: Issue to create profile for INR18650A battery in BQStudio

Part Number: BQ27Z561
Other Parts Discussed in Thread: BQSTUDIO, ,

Hi,

I am using a BQ27z561 fuel gauge. I have also purchased BQ27z561EVM-011 for developing profiles through BQStudio. I am using a total 6- INR18650A batteries. I want to create a profile for this battery pack (6 series). So, I am confused to set parameters in BQStudio to create a golden image file. I have mentioned the battery parameter below for a single battery pack. 

 INR-18650A single-cell parameter:

i. Configuration  Data  Design Voltage = 3600 mV
ii. Configuration  Data  Design Capacity = C =2500 mAh
iii. Configuration  Data  Design Energy = 9000 mWh
iv. Configuration  Data  SOH Load I = typical discharge current = ???? (Do not know)
v. Configuration  Charge  Charge Voltage = 4200 mV. 
vi. Configuration  Charge Termination  Taper Current = C / 20 = ???? (Do not know)

Can you please guide how can I use this parameter for 6 nos battery? Which parameters are multiply or add for BQStudio? Please suggest to me how can I go further.