This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176-Q1: LM5176 -constant current circuit - link to COMP

Part Number: LM5176-Q1
Other Parts Discussed in Thread: LM5176

Hi TI expert:

Quesiton: While the simulated circuit refer the below circuit, the constant current can't be lower. 

e.g The setpoint of constant current is 2.5A, but the simulated current is around 3.5A at 5A load. Evan it is setting lower (1A), it is also 3.5A.

The reason is there is a 0.25V Vf between Comp and op-Amp. So the comp voltage can't be pull down to 0V by op-AMP.

Do you have any idea?

Thanks.

Aska