Other Parts Discussed in Thread: TPS23880,
We have been using the TPS23861 in our products for some years now with good results. However we seem to be experiencing an increasing number of unexplained field failures. The failed parts are unresponsive on I2C and there is no detection activity on any channel. They are not warm to the touch. The vast majority of them have a characteristic mark, which can be seen in the somewhat fuzzy picture below. There is a crater just below the P and the S in the TPS marking. Most of our applications are outdoors, and some failures can be explained by lightning strikes, but this doesn't cover every case by any means. When no other visible board damage has been found, replacing just the IC has restored normal operation in every case. Does the location of this crater give any insight on what might have failed and why? We are phasing in an updated board using the TPS23880 to add 802.3bt support, but we have an installed base using the 23861s. Many thanks and best regards, Charlie