Other Parts Discussed in Thread: LM25116,
Tool/software: WEBENCH® Design Tools
Hi,
I need to design a IBB supply with following parameters,
Input voltage= 24-30 Vdc
Output Voltage= -22.8 Vdc @ 2 A
Controller= LM5088MH-2/NOPB
The problem is TI WEBENCH recommends a different values of components and SNVA856A recommends different.
Can you recommend, what source should I follow? WEBENCH or SNVA856A?
I have also attach a excel file in which a have calculated the components value with two different sources SNVA856A app note and Datasheet. I have also attach the WEBENCH solution below.
Regards
Zain
https://webench.ti.com/power-designer/switching-regulator/customize/67