This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5012EVM: LP5012EVM unable to communicate with LP50-1.1.1_EVM as I cannot set correct I2C address

Part Number: LP5012EVM
Other Parts Discussed in Thread: USB2ANY

In order to communicate with the LP5012EVM board I need to set the I2C address in LP50 to 0x14.

The "Latest Version" (v1.1.1 (2c26f1)) will not accept this as a valid address "stating it must be 0x28, 0x29, 0x2A or 0x2B".

Since the USB2ANY is using this as a 7-bit address, with 0x28 the physical bus sends I2C bus 0x50 (shifted 1-bit to left).

All forums replies from technical support state in the latest version of LP50 you can set address to 0x14, this is NOT the case.