Hello all,
I am using BQ76925 with 6 Li-Ion cells. I have two issues with the current measurements.
1. My current measurement is very fluctuating (up to 400mA).
2. when I reach zero current after the current is applied, the SENSEN and SENSEP are not equal.
I tried to recalibrate the SENSEN then only it becomes equal. How frequent should I update the SENSEN and should it be with respect to current or Temperature?
How to reduce the fluctuation and also the drift? is recalibration of SENSEN is the right solution?
Thank you in advance.