This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62745: Selection request

Part Number: TPS62745
Other Parts Discussed in Thread: TPS62125, , TPS62175

Dear expert,

My customer is selecting a buck converter for 4s Li-Mn battery power application, here are their needs:

  • 15Vin,3.3-5Vout, >=300mA
  • low Iq (TPS62125 is too large for them)
  • high effieicency 

Do we have similar ultra low Iq device like TPS62745? Thanks for your support.

  • Hi Minqi,

    TPS62125 is a good solution for this specification.  TPS62175 is a much wider VIN device and does higher Iq's of 22uA on normal operation but with load currents lower than 1mA you can use sleep mode to get 4.8uA Iq.  Hope that helps.

    Regards,

    Amod