This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53647: 1V Two Phase 45A power supply shuts down frequently

Part Number: TPS53647
Other Parts Discussed in Thread: CSD95372BQ5MC,

We are using TPS53647 from TI as core voltage controller and  CSD95372BQ5MC as buck converter in two phases.
We are facing an issue that the supply shuts down frequently.
Vout=1V
Iout_max=45A, VOUT_DC+AC ripple=3%  Iout_step=50%  Load transient=5%
Can you help us in reviewing the schematics.
Can you point out any issue in the schematics that could be causing this particular issue.