Hello,
Can I use TPS63020EVM-487 to derice a peltier cell?
If not, what is the proper driver/evaluation board for this application (driving Peltier)?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can I use TPS63020EVM-487 to derice a peltier cell?
If not, what is the proper driver/evaluation board for this application (driving Peltier)?
Thanks
Hi Jasper,
Sorry for the late reply, did not see your message.
Regarding the input voltage, are you referring to the voltage powering up the TPS63020EVM board? if yes I can use up to 12V if it is needed
For my application, I plan to 3-5 volt and maximum current less than 1 A or 2A depending on the type and number of Peltier cells that I have.
As this is the first time to use this board, please let me know the feature of the board:
1) input voltage range (power input)
2) output voltage/current limitations
3) Is it a current control or voltage control?
4) if I can feed the temperature to the board and use it as a closed-loop feedback system.
Best,
Vahid
Hi Vahid,
the answer of your question can be found in the datasheet of this device and the user guide. please spend some time on the documents.