Hi Ti support members,
I found when I pulg out Adapter,the REG08 value is still 0x74,VBUS_STAT is 011,CHRG_STAT is 10.
How can I juede there is no input device and charging stat is discharging?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti support members,
I found when I pulg out Adapter,the REG08 value is still 0x74,VBUS_STAT is 011,CHRG_STAT is 10.
How can I juede there is no input device and charging stat is discharging?
thanks
Hi Eric,
What are the components and values between BTST pin and SW pin? -- there is 47nF Capacitor.
How much capacitance is there on the input? -- the capacitor is 22uf+1uf+100nf
Can you measure the VBUS voltage and check the SW waveform after unplugging the adaptor?
--when I plugout the adapter,VBUS voltage is 3V, VBUS woltage is 12V when plugin the adapter.
you can check SW waveform from the jpg.
Hi,
1. Did you measure VBUS voltage at the VBUS pin? Is it 3V?
2. What are VBAT (voltage at BAT pin), IBAT, VSYS, ISYS before and after VBUS power source is removed?
3. Could you please provide all register values before and after VBUS power source is removed?
4. Please visit https://e2e.ti.com/support/power-management/f/196/t/890624 for I2C controlled BQ2560X: Schematic Review and PCB Layout Design Tips.
Thanks,
Ning.