Hi
As suggested by ApplicationReportSLUA609 I have a build of 555 + 4015 I use
4015 integrated FEED should be 5V or 3.3 volts
which should be your opinion
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
The switching threshold for the SYNC pin are about 2.25V so the device will work from either a 3.3V signal or a 5V signal - it makes no difference to the controller so it comes down to your choice and whatever voltage rails you already have in your design.
Regards
Colin
Hi - I'm glad I was able to help you make a decision. I'm going to close this thread now but please feel free to contact us again if you have any further questions.
Regards
Colin