Could you please give me any advice to synchronize two LMZM33604s (+15/-15V) with an oscillator? The oscillator must support two shifted outputs (0°/180°).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you please give me any advice to synchronize two LMZM33604s (+15/-15V) with an oscillator? The oscillator must support two shifted outputs (0°/180°).
Hi Thomas,
Can you describe your application? As for using the LMZM33604 in an inverted buck boost topology, refer to this app note for more information.
Also attached are some references to phase shift oscillators. This could be a starting point for creating a phase shift oscillator that could synchronize to the two LMZM33604s.
Regards,
Jimmy