This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5000: /SHDN pin's internal circuit.

Part Number: LM5000


Hi,

Related /SHDN, He wants to control LM5000-3 device using /SHDN pin from MCU.  Under power-up condition, he wants Low on /SHDN pin, and output high from MCU to wake-up LM5000-3.

Does /SHDN pin have pull-up resistor internally?  If yes, please let me know the resistor value.

The reason why we need it is to decide the pull-down register value on his actual board.

Thank and best regards,
M.HATTORI.

  • Hello Motoyasu,

    The voltage on this pin needs to be below 0.3V. If the pin is pulled to GND and the input voltage is at 12V, -2uA are flowing into this pin maximum, so a resistance of 150 kohm should keep this pin below 0.3V. to be on the save side, I recommend to use a resistor below 100 kohm and if you do not mind the current consumption 10 kohm is a nice value there.