Other Parts Discussed in Thread: BQSTUDIO
Based on the original question, I now understand that Reserve Cap IT Cfg setting will "reserve capacity setting will show 0% Remaining Capacity at the point the battery has the amount of reserve capacity specified." However, if Android shuts the phone down based on 0% SOC, not reserve capacity, how can this work? I ran a discharge test via GDK board controlled by bqStudio to terminate on 0% SOC. But that termination point did not reserve any capacity.