Related to the earlier post regarding LM5155 grounding: I see the same issue in LM5155 datasheet Figure 51. This shows a recommended layout. Because the Rs current flows into PGND it seems reasonable that Cf would be connected to PGND.
But I am surprised that Ccomp is connected to PGND and not AGND. Rfbb is grounded to AGND so I think the E/A is referenced to AGND.
Should Ccomp ideally be connected to AGND? I could wrap compensation components around from pin 6 to pin 7.