This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24735: BQ2473x software not detecting device

Part Number: BQ24735
Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ24725A

Hi,

We are migrating our setup to a new computer.

Previously we had installed on another computer BQStudio & Bq2473x Test Bench software and it worked (and still does) with our EV2400.

But when migrating to the new setup, we can use BQStudio without problems but the Bq2473x or Bq2472x softwares always gives us the same error, USB Error. Insure USB cable is connected and Driver is working.

We try to connect to a Bq24725a from the EV2400 it works with one computer but doesn't on the other one.

We installed the following :

- BQStudio 1.3.86

- EV2400Updater-0.28-windows-installer

- EV2400_Support_Components_20110524

Any help would be appreciated.

Thanks,

AM.