Other Parts Discussed in Thread: UCC24612, ISO7710
Refer to TIDA-01622 DOCUMENT.
Due to doubts about reflow assembly of SMD exposed GaN part, we had to take a different route to verify if all connections are soldered. And that involves applying a pulse at PWMH & PWML in turn from an external source. We have removed the controller, bias from HV side ( through the depletion MOSFET & resistor to SWS pin) - both were blown when the controller did not start up( for many reasons - ours is the first pcb).
We are almost about to reinstall the bias circuit - without the controller. But I think that wont work. Here is my thinking: The depletion MOSFET+ resistor with clamping zeners work safely only when the UCC28780 is installed because in correct mode of start up, the controller shuts off CPC3909 THUS preventing high current to go through the resistor & the clamp. So without the controller operating correctly, we will blow the MOSFET & the resistor, right?
So question is: how do we test an assembly to verify that all parts are of correct values thus a guarantee UCC28780 will start up correctly?
Is there a way to get pulses from UCC28780 in open loop?
robin