This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LP8725 PMIC has a 'BUCK2_FLAG MASK' bit (bit7) in BUCKCONTROL (0x0C) register
We are finding that if this bit is changed from 1 (mask the BUCK OK flag) to 0 (no masking of BUCK OK flag)
this causes the PMIC fault detection functionality to assert its RESET_N output, resetting our MCU - which it shouldn't if BUCK2 is OK.
BUCK2 is our always on MCU VDD_1V8 supply
'BUCK1_FLAG MASK' can be in either state without causing a reset.
BUCK1 is unused and disabled by our MCU firmware
However if BUCK1 regulator is changed from disabled to enabled, then the 'BUCK2_FLAG MASK' bit can be unmasked without causing a reset.
Again 'BUCK1_FLAG MASK' can be in either state without causing a reset
Aivaras,
I have assigned this question to the expert on this device, and I expect you will receive a response by end of day (US Central time).
Hi Aivaras,
Can you please provide a scope shot of this RESET_N behavior after disabling BK2_FLAG MASK? Please show at least the following signals:
Thanks,
Gerard
Attached is a trace of I2C write setting BK2_FLAG MASK bit to 0 and subsequent assertion of RESET_N 30ms later
PMIC_nRESET_OUT is LP8725 RESET_N [digital trace]
PMIC_EN is LP8725 EN/PWR_ON [digital trace – always high]
VDD_1V8 is LP8725 BUCK2 output voltage
PCIe_+3V3 is LP8725 VIN
The test jig used for this measurement is showing more noise than actually present on this voltage ..
Channel 5 and Channel 6 are LP8725 I2C interface
After a further 30ms there is a glitch on BUCK2 output voltage – is this PMIC restarting ?
[see second zoomed in waveform]
and after 30ms more RESET_N de-asserts ..
Hi Aivaras,
Thank you for providing additional details.
Please allow me some time to investigate whether we have any hardware to reproduce this behavior. I will get back to you with an update tomorrow.
Thanks,
Gerard
Hi Aivaras,
Unfortunately we do not currently have hardware at our Dallas site. I am checking with our Finland team and will provide more information early next week.
Thanks,
Gerard
Hi Aivaras,
I apologize for the delay. Our Finland team also did not have any hardware available, so we have scheduled a build of some EVMs to investigate this issue.
Thanks,
Gerard